You are here: Getting Started > Advanced Project Creation > Define Scheduling > Periodicity

Periodicity

The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input Pipe Block.

Set the Period of Execution

Figure 4-50: Set the Period of Execution

All the pipe values are computed independently of events and sequences execution.

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™